This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tina-ti plot current output



Hi, I'm trying to plot a current output

I'm using a voltage generator to generate pulses, I want to see how current varies in response to voltage.

Currently the output is in voltage, how do I switch to current?

(In virtual oscilloscope, I can only choose channels between VM1, VM2 etc)

Thanks a lot!

  • Esme,

    You can use the current arrow or amp meter to measure current. The waveform will be plotted in the diagram window. The oscilloscope does not have a current probe option.

    If you choose the Separate Curves option from the View option in the Display Window, the curves will appear in their own plots with scales adjusted automatically. If you want to do this automatically, simply rename one of your meters (voltage or current) and add a :1 at the end of the name (for example, AM1 would be AM1:1). This will tell the display window to use the Separate Curves option automatically.