Hi.
I have a newbie type question in relation to one of TI's design projects, "TIDA-00879_4.5 Digit Low Power Handheld (DMM)".
Referring to the schematic "tidrmi4.pdf", what is the purpose of U3, an OPA333. It seems to me if I try to measure 60V between J6, and J8, then current would flow through the low output impedance of the opamp? and 60V applied to the cpu, or have I missed something? How does this also influence current measurement.
Thanks