Other Parts Discussed in Thread: OPA211
Simulating an OPA2111 in TINA as a voltage follower with +/-5 volt supplies. According to data sheet CM input range is (V-)+1.8 to (V+)-1.4, so it should work for inputs between -3.2 to +3.6. With a simulated +2.8V input, TINA shows output of 1.7V (should be 2.8V). What's going on? Bad model, bad TINA or bad me?