I have a few hopefully softball questions about TINA-TI.
1) Is it possible to annotate a schematic with basic graphic elements like boxes, and arrows? All I can add right now is text and wires.
2) If I put a graphic (png) in a schematic, then put some schematic text on top of that, the text gets lost behind the graphic when I click on the graphic. There doesn't seem to be a send-to-back feature. Is there a better way?
3) One of my subcircuits/macros specifies a voltage meter (and uses this voltage internally). When I run the full simulation, these voltages show up in the diagram window though they are not desired. Unlike a voltage source I place myself graphically, simply set the output to 'None' in these macro specified sources.
4) I can create a macro from a netlist, and place that inside a schematic. Is it possible to create a macro from a schematic and place that in another schematic? I think the answer is no since macro pins are only available in TINA Pro?
5) For diagram outputs, it would be nice to order the curves. The way I do this right now is I prefix the name of each element with a number, e.g. 0_Vgen, 1_I_load, 2_Vout, etc. Is there a better way to do that?
Thanks,
Matt