This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00355, 400W battery charger : Purpose of external MCU

Other Parts Discussed in Thread: UCC25600

Hi,

I have a question about TIDA-00355. The TIDA has an external MCU in it's block diagram. The FB pin from MCU directly control the RT current of UCC25600.  But I have no idea the purpose of the MCU because the design realize CC/CV control with TL103 and it wouldn't require MCU control. Is the MCU a idea or option for user who would like to control by digital solution?

Regards,
Nagata.