Hello-
After updating the 'OPA657.lib' SPICE file today (but not the symbol), I got an error about not all pins of a subcircuit being present. So, I took a peek into the 'OPA657.lib' file with an editor (vim), and saw that the newest file has introduced and extra pin labeled 'PD'. My guess is it is "Power Down." Trouble is, the datasheet for the physical OPA657 list no such pin in any package!!!! (You can verify it yourself: Download the zipped software bundle for the OPA657, extract 'OPA657.lib', and with the editor of your choice search for the string "OPA657" without the quotes until you reach the subcircuit definition.)
I am using the new 64-bit LTSpice ⅩⅦ, the Windows version, which I am running in Linux via the wine Unix-to-Windows interface layer. (I guess now that ADI is buying Linear Tech, you should not be adverse to LTSpice!
My LTSpiceⅩⅦ had no problem running with the old symbol and old 'OPA657.lib' file (LTSpiceⅩⅦ is backwards compatible with LTSpiceⅣ); it just that some overload (non)recovery of the OPA657 was weird. I have double-checked my work before deciding to bother you, so I am reasonably certain there is something wrong with the 'OPA657.lib' file. Can you help?
Thanks and Best Regards,
-Tim Starr on behalf of GF@In