Hi
I simulated LMR23625 under Vin_min=16V, Vin_max30V, Vout=3.3V,
Iout=2A, but I couldn't simulate by reason of te error of "Failed Minimum Ton".
The figure4 is measured under Vin=36V, Vout=3.3V, Iout_max=2.5A.
Is this reason Webench's error or the out of spec of this device?
Best regards,
Yokota