Part Number: TPS2491
Other Parts Discussed in Thread: LM5069
Tool/software: Webench
Hi Team,
Customer are planning to use TPS2491 for their new project, but there is some limitation in this IC. Customer cannot set the output limit current up to 15A using the Webench Designer. The limitation is due to Webench Designer or the IC itself cannot handle such amount of current?
Customer requirement is as follows:
Vin = 47V-49V
Iout = 15A
Besides, we propose an alternative part which is LM5069 and they are able to run the Webench Designer per above requirement without any issue.
Kindly advise if TPS2491 can take 15A current limit or not.
Thanks.