Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hello,
We want to create from a +/-15V a +/-18V power supply (current needed is about 1A on each side). The GND is needed !!
Here is the topology we are thinking about:
The problem/question I have is on the LMZ34002 !!
It should work but I'm not able to make the simulation with this configuration.
With normal configuration I'm able to simulate with LTspice and also your WEBENCH but as soon as I try to use how we want to implement it, it don't work.
With LTspice this one is really slow, with WEBENCH I don't have good result and the simulation is too FAST.
Here are my questions:
1. Is it an issue to use LMZ34002 as shown as above ?
2. How could I make the simulation work then ?
Many thanks.