Tool/software: Webench
I am working with TPS54202 and I have question about the minimum value of the output inductor .
Design inputs: VinMin=14V, VinMax=24V, Vout=7.3V, Iout=1.0A
With WEBENCH® Designer TPS54202 program calculate inductor value L=6.8uH.
Eguation 8 in Data Sheet TPS54202 recommend inductor value Lmin=34uH.
Help please select target value output inductor. Thank you!