This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Webench/LM3429: Output current regulation

Part Number: LM3429

Tool/software: Webench

Im using LM3429 for boost led driver with constant current

Vin=11-30V

Vout=36-40V

Iout= 1.5A

In 12Vin I dont have the 1.5A, the max output current is 1.2A

From 15V-30V I have the desired output current 1.5A

Please help me