Part Number: LM5118EVAL
Other Parts Discussed in Thread: LM5118,
Tool/software: Webench
Hello,
for an application with Vin from 8 to 75 VDC I have developed an identical circuit board to the all'evalution board LM5118EVAL. The maximum current in each case is always less than 2.5A, while the external temperature can reach 50 ° C. So far in 2 cases of 100 boards in use, it has broken the integrated LM5118, is there a configuration problem with the current loop?
I noticed that with the WEBENCH simulator it's not longer possible to do the simulation of this component with these input voltages and output currents greater than 2A, should I to redesign the device for currents less then 3A?
Thank you
Mario