Other Parts Discussed in Thread: SN74AVC4T774
Hi,
When I have tried IBIS model assignment for TS3DV416, there are some errors which I have included below:
C:\Users\bgh38753\Desktop\sim\ts3dv416.ibs:
Success : Parse succeeded on file C:/Users/bgh38753/Desktop/sim/sn74avc4t774.ibs.
Success : Parse succeeded on file C:/Users/bgh38753/Desktop/sim/853S01I.IBS.
Warning : at line 206 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Only the first combination from the [Series Switch Groups] will be used.
Error : at line 221 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 222 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 223 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 224 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 225 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 226 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 227 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 228 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 237 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 238 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 239 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 240 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 241 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 242 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 243 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : at line 244 in file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs : Component TS3DV416DB_DGV has duplicate series pin mapping entries.
Error : Parse failed on file C:/Users/bgh38753/Desktop/sim/ts3dv416.ibs.
How can I remove this error?
Regards,
Bhavya