Tool/software: WEBENCH® Design Tools
Hello,
Regarding to Inductor current ripple of LM5018 on WEBENCH, I have a question.
My condition:
Vin=55V,Vout=46V,Iout(max)=30mA, fsw=544kHz
Generally, the inductor ripple current(typ) is following.
Inductor ripple current (typ) = 0.3(30%) x Iout(max)
In this case, 0.3 x 0.03A = 0.009A(9mA)
But according to WEBENCH, it is shown as 0.042A(42mA).
Please refer below capture.
I am wondering why there is different each other.
Which should I believe?
Or on WEBENCH, is it calculated by other formula?
About inductor and output Capacitor on WEBENCH,
Is it base on above parameter?
(Peak-to-peak inductor ripple current)
Regards,
Tao_2199