Part Number: TLV61220
Other Parts Discussed in Thread: TPS61220,
Tool/software: WEBENCH® Design Tools
The product page says to download the SPICE model from WEBENCH, but WEBENCH doesn't include the TLV61220 or TPS61220.
They are recommended by power quick search:
But when I click "WEBENCH Design" they are not listed.
If I launch WEBENCH from the product page itself, it seems like my values are ok:
but then it says it can't work because of current limit:
It's calculating an Iout of 204 mA instead of the 15 mA I specified?