Part Number: TIDA-00650
We have manufactured TIDA-00650 boards using the provided design files. I have modified the lookup table and J1 connector for using a T-type thermocouple. Since the voltage output of T-type is within the same range as K-type, the filtering components are unchanged.
I have tested up to 5 boards with two T-type TCs and experiencing large board-to-board differences in accuracy. The swing is anywhere from 0.15C to 1C with respect to a reference Agilent data logger. I have validated that the board accuracy remains the same by swapping TCs thus eliminating TC inconsistency.
I would appreciate any input on where I should focus my attention to understand the reason behind these large swings. Thanks!