This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi,
I was assigned by a project. Which is ac/dc converter based on TI chip. IC number is UCC28070. From TI portal i was found TINA model of UCC28070. But there are three pins mismatch in the application schematic .
In datasheet three pins are used i.e.CDR,RDM and GND instead of these three in application schematic three other pins used i.e. IRIPA,IRIPB and f_KHZ.For my project work need the IC as in the datsheet. Please support me to get it.Application model and datasheet attached here5826.ucc28070 datasheet.pdf0602.slum328.tsc
Harijarani,
Arash has linked an explanation of the additional pins in your other post and the CDR and RDM pins are not present in the model because they are not being used in the TINA-TI model. It appears that the frequency dithering is not offered in the PSpice model and that was used to create the TINA-TI model.
If you have access to Simplis, we might be able to provide you with a Simplis model for the device.
Harijarani,
Please send me an email address where I may contact you directly.