Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
I have downloaded the Spice file for 'LM2733' from Ti - WEBENCH Designer(link mentioned below)
Also I have attached the 'Tina-Ti spice model' which I have downloaded from the above link.
But the file I got is in 'Encrypted' format. I cannot able to use the file in my tool.
Can I able to get 'Decrypted' version of the same file, which I have attached?
Or Could I get a Spice file for Boost converter IC - LM2733 in txt format?
Ø Boost converter IC configurations :
- · Vin - 12V
- · Vout - 18.2Vmin to 24.8max
- · Imax - 200mA.
Kindly do the needful.