Part Number: TIDA-00120
Other Parts Discussed in Thread: MSP430F5132
Tool/software: Code Composer Studio
I have used the TIDA-00120 design as reference. I used Code Composer to compile the code given in the software files. When building the code, I get an error saying 'Program "make" is not found'. I tried this solution (https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/373261/1313023#1313023) but the "${CG_TOOL_ROOT}/include" already existed. However, it seems like the code builds and finishes as if normal. Ignoring this error, when I try to connect to the GUI, it initially connects, the program freezes, then disconnects after a few seconds saying "Connection Lost (IO)!". I have tried many people's suggestions for fixing it including commenting out the "//" in "//#define GUI", switching pins around, etc.
Below is a picture of how I have it set-up when connected for GUI, please let me know if it is even set up correctly. I am using a MSP-EXP430G2 board and a MSP430F5132. The Vcc pin from the MSP-EXP430G2 is connected to the VCC pin on the J5 connector of the charge controller board, Tx is connected to Led3 of the J5 connector, Rx is connected to Led2 of the J5 connector, and the two ground are shorted together on the J5 connector.
I have tried many things including different computers and even different version of CCS. Please answer back if you have any idea of the issue.