Part Number: OPA627
Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hi All,
The attached circuit exhibit wrong noise analysis. Is this because of spice model of OPA627 or software limitation?
Kind regards
Jubayer
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jubayer,
It looks like the resistors are affecting the noise sim results.
A second circuit was added to your TSC file. The revised file is attached to this thread.
In the second circuit, the resistors were replaced by voltage-controlled current sources (VCCS).
They act as equivalent resistances, but don't contribute noise to the circuit.
A noise sim shows the input-referred noise for the new circuit is 4.82 nV/rt(Hz), which is close to the voltage noise in the datasheet.
The TINA plot is shown below.
I hope this helps. Please let me know if you have any questions.
Regards,
John
Jubayer,
An AC sim shows the forward gain in the pass-band is -2.77dB, so it makes sense the input-referred noise is larger than the output noise.
With the reported output noise (169nV/rt(Hz)) and gain, the corresponding input noise should be 169*(10^(2.77/20)) = 232 NV/rt(Hz).
So the TINA sim seems to be working fine.
The simulation results are different from the hand calculations because of the input capacitance of the op amp (model).
The total external capacitance at the noninverting pin to ground is 4pF. Simulations show internal capacitance of the noninverting input is about 7.1pF which is consistent with the data sheet value of 7pF.
My hand calculations show that with 4pF of total capacitance, you get 442nV/rt(Hz) of output noise for your circuit, which is close to your result.
If you take into account the device/model input capacitance of 7pF and add that to the 4pF of external capacitance, the calculated output noise drops to 164 nV/rt(Hz), which is pretty close to the 169 NV/rt(Hz) sim results.
When you increase the external capacitance to the nF range, the device/model input capacitance becomes negligible and the calculations need only take the external capacitance into account. That's why your calculated results for 2nF caps agrees with the simulations.
So it looks like the OPA627 model aligns pretty well with the data sheet specs.
The TINA noise simulation seems to agree pretty well with theoretical calculations, so it seems to be okay as well.
I hope this helps.
Please let me know if you have any more questions.
Regards,
John
Dear Mr. John,
I would like to thank you for your explanation and useful solution.
Now, to verify the output noise of the attahced new cirucit (OPA627 in inverting mode), sim result shows output noise of 61 nV/rt(Hz) at 10KHz. By hand calculation, I found 64.72 nV/rt(Hz) at 10KHz considering only two external capacitance of 2 pF. Now, for this configuartion, if I take into account the device/model input capacitance of 15pF (differential i/p cap. + CM i/p Cap from datasheet) in addition with two external capacitors , my hand calculation shows 68.4 nV/rt(Hz) at 10KHz exhibiting significant difference from the hand calculation.
Now my questions is:
1. Why does the hand calculation of 64.72 nV/rt(Hz) at 10KHz show the good agreement with the simulation result of 61 nV/rt(Hz) at 10KHz even though the device/model input capacitance of 15pF (differential i/p cap. + CM i/p Cap) is disregarded in the caluclation?
Look forward to hearing fro you soon.
Kind regards
Jubayer