This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi,everyone:
Could anyone tell me why I can't edit my schematic in power design with LM5022? thank you !I need your help.
I need a isolated power supply which outputs ±2.8V with 2A load. WEBENCH gives me a schematic with LM5022.But it need to be edit. however,I can't find the icon "EDIT",I can't edit it.
I have read the instruction very carefully.but i don't have the link"edit" to edit my schematic.do i do something wrong.
The Edit Link is only available when the native Electrical Simulation is enabled in WEBENCH which is not in case of the Isolated Flyback.
The alternate to edit and simulating in WEBENCH is to use the TINA-TI model on the web. TINA-TI allows you full free form editing capability.