Tool/software: TINA-TI or Spice Models
I can't seem to get the X-Axis to scale to what I want. If I run a simulation with a 100uS 3.5Volt peak triangle wave and set the analysis mode to Transient with an end time of 102uS the diagram window plots a 1ms X axis.
If I double click the X-Axis and change the upper limit to 100u it will then change the axis to 100uS but if I try anything between 100 and 109us it doesn nothing and stays at a max upper limit of 1ms.
If I type 110us it then changes the axis to 200uS.
I really don't understand what is going on with this or how to make it do what I want. Anyone have any ideas?