Tool/software: WEBENCH® Design Tools
Hello Webench team.
I am trying to run a design from Webench in the TPS61170 product folder.
Vin 5V, Vout 36V 5mA.
Webench opens.
Says Design cannot be created with this device.
However if I click OK on the box that pops up and then click RECALCULATE, without changing the parameters, a list of usable devices is shown.
One of them is TPS61170-Q1, which is the same device as TPS61170 but auto qualified.
I can click on the Q1 part and get a full design.
If the design will work with the Q1 it should work with the standard part, I believe.