Tool/software: WEBENCH® Design Tools
Hi
I simulated TPS55340 with the following condition by WEBENCH.
As the results, the Cin was selected a alminium capacitor such as 22uF(ESR:1.2ohm).
Can we use the alminium capacitor such a high ESR for Cin if the Vin_ripple is accepted for the application?
Vin=24V(+/-10%)
Vout=32V
Io=0.5A
Regards,
Koji Hamamoto