Part Number: LMZ31503
Tool/software: WEBENCH® Design Tools
Hi Guys,
I am trying to use LMZ31503 in a design from 12V-5V at 3A in EAGLE 7.7.0. I downloaded the webench design(including library files) and when i tried to execute the script and follow instructions as provided in this post (e2e.ti.com/.../355494), i received errors such as
"Can't place pin PVIN_3 on pin PVIN_2!; Can't place pin PVIN on pin PVIN_2!; Can't place pin INH_UVLO on pin INH_UVLO_2!; Can't place pin VOUT_3 on pin VOUT_2!; Can't place pin VOUT_4 on pin VOUT_2!; Can't place pin PH_3 on pin PH_2; Can't place pin AGND_3 on pin AGND_2; Can't place pin PGND_3 on pin PGND_2!; "
Because of the above errors, I am not able to tie all the VOUT pins together, or PH pins, or AGND pins, or PGND pins, etc. which is obviously a problem.
Can you please let me know what has to be done here or where am I going wrong?
Thank you,
Rinald Pereira