Hi, I need a chip that is easy to use with a frequency that can be set with an R and/or C to produce an output sequence of 1 0 1 0 1 0......., essentially an oscillator or clock. It needs to be able to operate at fairly low, power system speeds.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I need a chip that is easy to use with a frequency that can be set with an R and/or C to produce an output sequence of 1 0 1 0 1 0......., essentially an oscillator or clock. It needs to be able to operate at fairly low, power system speeds.
Hello Del,
See page 13 of the LMV761 datasheet: www.ti.com/lit/ds/symlink/lmv761.pdf . The LMV-series is low power, hopefully the frequency you need can be generated with this simple circuit.
~Leonard