This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools: TPS54526PWP: Feedback resistor selection

Tool/software: WEBENCH® Design Tools

Hi,

I'm using TPS54526PWP in my design for 1.35V generation from 5V input.

The schematics is attached below.

The Webench schematics is as below.

The confusion  I have is, whether to use the feedback resistor I have in my schematics are ok or do i need to go with values suggested as in Webench schematics.

Please let me know ASAP.

Thanks & Regards,

Nanjunda M

  • Hi Nanjunda,
    The feedback resistor from either of the design should be ok to give you 1.35V Vout. The difference is only 1mV between the two. The WEBENCH resistor has a slightly higher resistance of 46.1K compared to 39K which can give you slightly lower leakage. But the Vout is 1.3512 V from an accuracy perspective. You can pick whichever you are comfortable with.

    Regards,
    Gerold