This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS54335A: Failure for 90% duty simulation

Guru 19645 points
Part Number: TPS54335A
Other Parts Discussed in Thread: TPS54334, TPS54334EVM-722

Tool/software: WEBENCH® Design Tools

I simulated TPS54335A's Webench on below condition, but  failure and indicate "Calculated duty cycle exceeds limit" .

I think that TPS54335A Webench data have a bug because I tried Low fsw condition but same results, please confirm it.

If it was bug, please let me know about revision schedule.

・Vin: 13.2V~21V

・Vout: 12V

・Iout: 1.1A

【Additional information】

・When fsw is changed low value (100kHz, 500kHz, etc), results was the same (duty cycle exceeds limit).

・TPS54335A datasheet is described "Min off time: 0%"

・TPS54334 was simulate normally, I feel that TPS54334 and TPS54335A are near specification.

Best regards,

Satoshi