This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM26420-Q1: WEBENCH

Genius 4840 points
Part Number: LM26420-Q1

Tool/software: WEBENCH® Design Tools

We would like to use WEBENCH using with LM26420X-Q1 at following 4 cases.

But WEBENCH doesn't work in these conditions.

 

CaseA

3.3V->1.8V(to 0.25A)

           1.5V(to 1.4A)

 

CaseB

3.3V->1.8V(to 0.53A)

          1.5V(to 1.4A)

CaseC

3.3V->1.5V(to 1.4A)

      1.2V(to 0.01A)

 

CaseD

5V->1.5V(to 1.4A)

    3.3V(to 0.14A)

 

 

We would like to get efficiency information and space information at these conditions.

Please help us