Tool/software: WEBENCH® Design Tools
Hi,
I am trying to use Webench for TPS54318 with the following specifications.
Vin - 4.5 to 5.5V
Vout - 3.3V
Iout - 3A
Webench is not able to simulate this part and showing an error - 'Maximum Power Dissipation = 0'
Is there any issue with webench or does the part has any issue supporting 3A?
Regards,
Praveen GD