This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/UCC28950: Transient model

Part Number: UCC28950
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

Hello,

I want to design a DC/DC 3kW SMPS using the UCC28950,

Input voltage: 370Vdc to 420Vdc.

Output voltage: 56V.

Output current: 40A maximum.

I see the steady example, but I want to use the UCC28950 transient model.

Is there an example that uses the transient model or is there the possibility to switch from steady to transient model?

Thank you.