Part Number: PMP20289
I noticed that in "PMP20289 RevA Test Report" document, on page4 it is mentioned that the inductance values for the transformer and the inductor is 67.5uH and 1.66uH respectively. The frequency of the measurement is said to be 400kHz. Here is my question:
Can you please explain about the measurement method/ device which has been used to get those uH numbers?
As far as I know at 400kHz of AC frequency, finding a measurement tool (e.g. impedance analyzer, LC meter etc.) which can give the required power for magnetizing the core, is very difficult. So I am really interested in knowing what you did in this case?
Bests,
Armin