This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM22679: Webench simulation problem

Genius 4220 points
Part Number: LM22679


Tool/software: WEBENCH® Design Tools

Hi,

I'd like to get the WEBENCH simulation result of LM22679 with following conditions,

Vin=35V Vout=26.5V  Iout=5A

But I couldn't get the result and got the comment "Output voltage not supported".

is there any problem for the condition?

Thanks

Go