Other Parts Discussed in Thread: TINA-TI, ,
Tool/software: TINA-TI or Spice Models
Hi, I am evaluating the LM5175 DC/DC controller. I intend to build a 8-36V input, 15V, 4A output power supply for an operating temperature of 85C. I designed the controller using bode analysis and am trying to simulate the TINA -TI model I downloaded using webench. The model simulates fine, as in I Can see the voltage and current at different points in the circuit and I can run it at rated load. But I want to view the frequency response of the system (output voltage to disturbance). I have inserted a supply VG2 between the feedback resistor and the output voltage rail. When I try to get the bode plot, the software throws up an error saying that it cannot find the operating point. I am wondering if this is due to LM5175 not starting right at the beginning (startup time) and therefore, the analysis is not completed. Anyway, I need help to figure out how to view the frequency response of the system. The TINA-TI simulation has been attached with this post for anyone who wishes to view that.LM5175_sim_up_tf_analysis.TSC