I'm using a few tps6300x devices (both variable & 002/fixed 5v) supplies on a new board, and wanted to create some models on Tina-TI (SwitcherPro works fine on the part). I see the PSpice files are recently available. I believe TINA needs both a '.lib' & '.tld' files. The PSpice package includes only the '.lib'. TINA is pretty smart & knows I'm missing the .tld file if I place the 'lib' in the 'C:\Program Files\DesignSoft\Tina 7 - TI\SPICELIB' directory & try to run. The startup error catches I'm missing the file, 'The number of LIB and TLD files in the SPICELIB folder must be the same'.
Is there any way I can use the available tps63002 PSpice files for modeling in TINA-TI, or is there a more recent example I can snag for that part series?
I'm XP-Pro sp3, core-2-duo desktop, 4gb ram, TINA-TI v7.0.80.96 SF-TI
Thanks for any tips - Steve