Hi folks,
I am using the TIDA-00195 reference design ( IGBT Gate Driver Evaluation Platform for 3-Phase Inverter System) IM application. With this design, the BOM was also included in the file. In the BOM, all the components are available from the respective vendors except a transformer (T2,T3,T4 in TIDA-00195) from Wurth Electronik. This transformer is neither available with vendor nor other suppliers. Please help me with the component details or alternative / equivalent to the existing component. I am also disclosing the part number & make of the transformer.
Transformer
Part Number :750342573
Make : Wurth Elektronik