Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hi,
Customers are trying to make inverting circuits using TPS62163.
Customers are considering circuits like the following materials.
Http://www.tij.co.jp/jp/lit/an/slva469c/slva469c.pdf
Can I simulate the inverting output (3.3 V -> -5 V / 60 mA) of the TPS6216x series with TINA simulation tool?
If yes, is there an inverting circuit model?
Best Regards,
Yuto Sakai