This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM26420: Question about inductance value

Guru 19615 points
Part Number: LM26420

Tool/software: WEBENCH® Design Tools

I trying to simulate Webench below condition,

--------------------------------

・Device: LM26420X(fsw: 2.2MHz)

・Vin: 4~5.5V

・Vout1: 1.2V / 1.1A

・Vout2: 3.3V / 0.6A

--------------------------------

But, for example, Vout2(3.3V) inductor's Lowerbound is 7.988μH, I feel that more small inductance is no problem.

What is the reason for inductor's Lowerbound: 7.988μH?

(Is this Webench bug?)

By the way; I hope to use 3.3μH inductor, and compensation was over 45° in the condition of 3.3μH.

Is there any problem for 3.3μH?

LM26420.pdf

Best regards,

Satoshi

  • Hi Satoshi San,

    For this design, Inductor value is calculated by considering the peak to peak ripple as 10% of Iout (The KIND value is 0.1) for both the channels. Please see the below equation. The minimum value will be little below what the equation calculates(Typically 0.8*Lo(min)). So the 7.988uH. 

    You can reduce the inductor value to 3.3uH, but it increases the peak to peak ripple current roughly up to 30% of Iout. Kindly take this into account depending on the type of load you're driving.  

    Best Regards,

    Bhushan