Part Number: TIDA-00267
Other Parts Discussed in Thread: SN65HVD255, TCAN1042-Q1
Hi,
Our customer is considering evaluating CAN_FD using TIDA-00267.
The signaling rate is assumed 2Mbps.
Although SN65HVD255 is on TIDA-00267, if it is replaced with a pin compatible CAN_FD product such as TCAN 1042-Q1, is it possible to use it without changing it altogether?
Should they need to change the circuit constant or change the artwork?
Best regards,
Tomoaki Yoshida