Tool/software: WEBENCH® Design Tools
Hi
I simulated TPS56121 the following condition.
But the results about Vp-p was different(1st time is 4.881mV, 2nd time is 7.454mV).
Could you tell this reason?
Vin_min=Vin_max=13V
Vout=10.5V
Iout=8A
Fsw=500kHz
Ta=90℃
Best regards,
Yokota