Hi, I am working on a consumer product that needs to brighten and dim a UV led which runs at 3-3.3 V at 10 mA. The circuit just needs to brighten and dim the LED every 5 seconds or so in order to conserve battery life. Is it possible to do this with a LDO (low dropout voltage regulator) or is possible to use just passive components?
Scot