This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMR16010: Can LMR16010 output stable 15V ?

Part Number: LMR16010


Tool/software: WEBENCH® Design Tools

The input voltage is 42VDC and I want to get 15VDC / 1A output. But WEBENCH cannot output a solution on LMR16010. Is it a problem about WEBENCH?  Who can tell me the input/output capacitor, inductor size? 

Thank you very much.