This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00364: TIDA-00364 changing 48VDC to 84 VDC ?

Part Number: TIDA-00364
Other Parts Discussed in Thread: CSD19536KTT

Hello,  TIDA-00364 48-VDC Battery Powered 5-KW Inverter Power Stage  :

How to change schematic to accommodate the battery voltage of 84 VDC (20S Lipo - 74V nominal, 84V fully charged)  given the same continuous current rating (hence increasing the power respectively)?  Power stage - half bridges looks like very capable up to 110v allowed on CSD19536KTT MOSFETs, all capacitors 100v  - looks very capable.  Sensors conditioning I will make my own according to the voltage, here my concern is only changes in the power stage.

If it is doable, Please point to the areas need changing (like resistor dividers, bootstrap circuits, etc...)

Thank you in advance

Vladimir