Part Number: TPS61087
Other Parts Discussed in Thread: TINA-TI, TPS61088, TPS55340, TPS55330
Tool/software: WEBENCH® Design Tools
Customer use TPS61087(Step-Up DC-DC Converter) for simulation, input voltage is 5V ,output voltage is 12V. From the datasheet we can see maximum output current is about 1.3A .
However, if we set output current 1.1A and change inductor and diode value(to meet the requirement of output current), WEBENCH didn’t work. The error message is shown as fellows.
The schematic for simulation is shown as fellows.
So the problem is why WEBENCH failed in this condition. Customer wants to know if output current is a little larger than 1A, what should we do?