Part Number: LM5122
Hello,
Below is LM5122 condition. But customer can not simulate by this condition on Webench. Has any problem for it? Does LM5122 support this power? Thank you.
Input:9~36V
Output:36V
Output Current 5A
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5122
Hello,
Below is LM5122 condition. But customer can not simulate by this condition on Webench. Has any problem for it? Does LM5122 support this power? Thank you.
Input:9~36V
Output:36V
Output Current 5A
BR
Patrick
Hello Patrick,
The desired design test conditions of
Input:9~36V, Output:36V,Output Current 5A
corresponds to a buck-boost converter and there is NOT WEBENCH solution.
If you make VinMin=VinMax-36V, Vout=35V, Iout=5A, there are several solutions and LM25085x are the highest ranked models.
Regards,
Flora
PS. Most WEBENCH solutions cannot reach Dmax=100% because our calculations include Rds(on), DCR, dead time and other losses
Hello Flora,
Below is customer condition. They have power source 12V~24V. IOUT=2A. That could be simulate design. But while change IOUT 5A, we can get the it. Could LM5122 not support IOUT 5A while 12V~24Vin ? Thank you.
BR
Patrick