Part Number: TIDA-00207
Other Parts Discussed in Thread: STRIKE
Hi team,
My customers are creating circuits based on TIDA-00207.
They are studying whether ESD protection element can be used as it is.
They request HBM 20kV or more in the system.
Is there a result of ESD test on the board of TIDA-00207?
I would like to know whether these ESD protection elements are capable of withstanding HBM 20 kV.
Best regards,
Tomoaki Yoshida