This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
We are designing a 15V, 3 A flyback converter ( I/P - 150 to 250 V, 50 Hz AC RMS). We are using the reference design from
webench for the power circuit and snubber alone and the pulse for MOSFET is given from an external MCU (C2000 launchpad).
But the voltage across the MOSFET has severe spike as well as ringing while using the same snubber values as in the reference design.
Pls suggest to resolve this issue.
We are using the below components, MOSFET - FQPF7N80C
Flyback transformer with a primary inductance of 750 micro henry
switching frequency - 80 kHz.
Hi Lenin,
Can you share the WEBENCH design with me (sahilg@ti.com)
I also want to look at the device which we are using for the above WEBENCH schematic.
Let me know if you face any issues while sharing the design.
Thanks
sahil