This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice: KR_DMLQ31.23

Other Parts Discussed in Thread: TINA-TI

Tool/software: TINA-TI or Spice Models

NONAME (TINA Netlist Editor format)
**************************************
**  This file was created by TINA   **
**         www.tina.com             **
**      (c) DesignSoft, Inc.        **
**     www.designsoftware.com       **
**************************************
.LIB "<TINADIR>\EXAMPLES\SPICE\TSPICE.LIB"
.LIB "<TINADIR>\SPICELIB\Operational Amplifiers.LIB"
.temp -40
.AC DEC 20 10 1MEG
.TRAN 2N 1U


IS1         0 1 226.3M
DLED1       1 0  D_binM

.MODEL D_binM D(IS=3.3351E-19
+ N=1.7876
+ RS=1.0901
+ EG=2.3424714469565
+ XTI=3
+ TRS1=-2.24239068344327E-03
+ TRS2=3.01638657411695E-05
+ CJO=0.0000000005)

.END

I have imported this netlist to Tina.  I find that the results over temperature do not match with LTspice.  From my analysis, it appears that Tina does not utilize the TRS1 and TRS2 parameters of the LED model.  Can anyone confirm if this is true or explain why LTspice does not match Tina at -40C?