Other Parts Discussed in Thread: LM22679
Tool/software: WEBENCH® Design Tools
Hello
I plain to use this LM22679 component for my power supply ,
I need 5,15v out so I plain to use the -5 version with external voltage divider .
End of page 14 of the datasheet says " A max value of 10k ohms is recommended for sum of Rfbb and Rfbt " ( and max 2k ohms for the -5 version )
When I use WEBENCH tool , the Rfb1 is given at 47.5k ohms and Rfb2 at 330 ohms
Should I follow webench or , the datasheet ?
Thanks