This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi TI Support,
I happened to create 15 to 3.4V design with Iout=1.5A. I followed the datasheet design steps. Most components are customized including compensating components. Design seems to be stable but cross over freq. in bode plots is not matching to Op Val. If anybody can provide email ID, I can share the design for your review.
Please advice.
Thanks,
jagdish
Hi Jagdish,
Thanks for the question. This has to do with the output cap being a custom cap and how sim and opvals are handling the capacitor's derated value for internal calculations. Both bode plot sims and opvals should be using the "Total Derated Cap" value that you observe when you set the custom cap properties ("Select Alternate part" -> "Create a custom part"). Currently, for your design, the total derated cap value is set to 55uF which probably got carried over from the default design. However, the bode plot sims seem to be using the nominal cap of 2 x 47uF = 94uF for simulation causing this discrepancy. I will need to look at it further to see why this is happening.
In the meanwhile, to get around this, you can set the "Total Derated Cap" to be the derated value of the custom cap you will use on the board. "Cap" = "Total Derated Cap"/"quantity in parallel". So, if you are using a 55uF value for Total Derated Cap and 2 caps in parallel, use 27.5uF for the Cap value. This way both bode plot sims and opval calculations will use same cap value internally. The "Re-Comp" feature uses the "Total Derated Cap" value and you can see this under "Power stage components" tab where Cout value is shown.
Here is a link to the updated design from you with 2 caps in parallel and using a total derated cap of 55uF and cap value of 27.5uF (as an example):
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=BCA49151749956AD
You can change the values as required by clicking on "Select Alternate Part" -> "Create a custom part". Please let me know if you have any questions. Also, if you would like me to change the derated value from 27.5uF to a different value, feel free to let me know and I can send an updated design link here for you.
Regards,
Amod
Jagdish,
Sorry I missed that issue. I refreshed the design and also ran the simulations here in this design: https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=497642EB30C2B944 It might have been an issue with a corrupt design while making all the custom changes. Please let me know if you are able to simulate input transient and startup sims now.
Regards,
Amod
Hi Jagdish,
I created a new design with your specs and matched each component one by one with your shared design.
Regards,
Amod